Keeping the hydro-energy flowing

Keeping the hydro-energy flowing

Grande Dixence reservoir and dam in Switzerland

/ THE GRANDE DIXENCE HYDROELECTRIC POWER STATION IN SWITZERLAND GENERATES ENOUGH KILOWATT HOURS OF ELECTRICITY TO MEET THE AVERAGE ANNUAL CONSUMPTION OF 400,000 HOUSEHOLDS. MAAGTECHNIC AG – AN ERIKS COMPANY – HAS PLAYED ITS PART IN ENSURING THE POWER STAYS ON.

Taking eleven years to build, the Grande Dixence dam and power station was finally commissioned in 1961. So when Maagtechnic AG was called in, the lubrication systems for the shaft bearings of the 17MW storage pump assembly were over 50 years old. Briefed to develop replacements, Maagtechnic faced the challenge of designing systems which would not only cope with the environmental conditions at 2,365m above sea level, but which also matched the mass and function of the old systems. And since a failure of the lubricant supply could result in a total machinery standstill, 100% reliability was essential.

A total of three Maagtechnic AG lubrication power packs were commissioned over a period of two years. The first of the innovative lubrication units has an oil flow rate of 220 litres per minute, and the other two a rate of 180 litres per minute. The systems are fed by a corrosion-resistant oil tank with a volume of 1,000 litres.

100% reliability was essential

With the updated lubrication systems now in place, the four turbines of the plant can continue to provide a quantity of hydro-electric energy equivalent to the output of a nuclear power plant – hopefully for at least another 50 years.

The UN Sustainable Development Goals and our Material Topics

UN Sustainable Development Goal: Affordable and clean energyMaterial Topic Icon Climate Change and Energy
close layer
cover of Sustainability report
Pre-register to get your copy of the ERIKS Sustainability ReportSalutation
Country

ERIKS NV respects the privacy of the visitors to this website. By filling this form you provide information about yourself, which may be used for marketing purposes. ERIKS is responsible for processing this personal information via this website within the meaning of the Personal Data Protection Act. Your information will not be provided to third parties.